This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Is there support for controlling the RS485 transceiver direction in the driver? My design uses Modbus over half duplex RS-485, and the transceiver direction needs to be set to drive the lines only during transmit. This needs to be disabled immediately after the last character leaves the UART. I see options for setting flow control, is there any way to use these features, or others, to implement the quick turn around of the RS485 driver? The other option is to write a custom interrupt routine and install it using the driver. Then the interrupt routine can handle the direction control. I would rather find a feature already in the driver instead of implementing my own ISR.
Hi Robert,
I will need some time to look into this. I will try and have feedback by the end of the week.
Thanks,
Alexis
Hi Robert,
Sorry for the late response. As far as I can tell there doesn't seem to be support for RS485 transceiver direction..but I'm trying to get confirmation on this. I'll let you know if I hear otherwise.
Thanks,
Alexis
**Attention** This is a public forum