Part Number: MSP-EXP430FR5994
Tool/software: Code Composer Studio
Hello,
I'm new to the MSP430. Using the MSP43fr5994 launchpad,
Using Code Composer Studio 9.1.0.00010
Code is based on 'BlinkLED...' example.
Code is compiling and running well (LED is toggled) but I'm not seeing any output of the puts in the CCS 'Console' tab.
What is missing?
#include <driverlib.h>
#include <stdio.h>
int main(void) {
volatile uint32_t i;
// Stop watchdog timer
WDT_A_hold(WDT_A_BASE);
// Set P1.0 to output direction
GPIO_setAsOutputPin(
GPIO_PORT_P1,
GPIO_PIN0
);
// Disable the GPIO power-on default high-impedance mode
// to activate previously configured port settings
PMM_unlockLPM5();
puts("Started");
while(1)
{
// Toggle P1.0 output
GPIO_toggleOutputOnPin(
GPIO_PORT_P1,
GPIO_PIN0
);
puts("1");
// Delay
for(i=100000; i>0; i--);
}
}
Thanks.