Other Parts Discussed in Thread: TAS2559
Hello,
customer wants to use the TAS2559 and MSPFR2153 but needs a I2S interface to connect the audio amplifier. Can it realise with SPI and SW like described in the app note?

Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
customer wants to use the TAS2559 and MSPFR2153 but needs a I2S interface to connect the audio amplifier. Can it realise with SPI and SW like described in the app note?

Regards, Holger
Hello Bruce,
so, you say with a device like MSP430FR5720 which has a DMA it should work?
Regards, Holger
It seems that way, at least as far as the DMA -- it has 3 channels (like the F5418) and triggers for all 3 (SPI-capable) eUSCIs [Ref Data Sheet (SLASE35C) Table 6-7].
Beyond that it's standard "due diligence". [Disclaimer: I haven't used the F5418 nor this AppNote.] I wasn't able to locate the associated code (.zip) to check for surprises. Based on the .pdf:
1) The F5418 has a 12-bit ADC and the FR5720 only a 10-bit.
2) It appears to rely on a 8.192MHz system clock, while the FR5720 factory-trimmed DCO selection has only 8.0MHz. I expect 2.4% makes a big difference in audio. Figure on using an external crystal (HFXT).
[Edit: Erratum DMA9 sounds like something that could get in the way. [Ref Errata Sheet (SLAZ373AE) p. 10]]
**Attention** This is a public forum