This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: Standard SPI slave

Part Number: MSP432E401Y
Other Parts Discussed in Thread: MSP430F5438A

Hi,

We are planning to upgrade the micro from MSP430F5438A to MSP432E401Y in one of our existing product.

Following SPI ports are being used in existing MSP430F5438A product- 

1. Two SPI slave ports , both configured as UCCKPH=1  and UCCKPL=0.

2. One SPI master port, configured as UCCKPH=1  and UCCKPL=0.

Struggling with MSP432E401Y's TRM QSSI section but not able to clearly understand if MSP432E401Y can support above mentioned master and slave configuration ?

Shall we consider MSP432E401Y as replacement (these two SPI configuration context) ? Where can I get the corresponding code examples ?

Regards,

Pradeep 

**Attention** This is a public forum