Part Number: MSP430F5438A
Hi
3.During RTC operation with a backup battery, the RESET pin is set to “L”.
Will this affect the RTC operation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F5438A
Hi
3.During RTC operation with a backup battery, the RESET pin is set to “L”.
Will this affect the RTC operation?
Hello,
Just to get on the same page here, the battery backup RTC functionality is available on the RTC_B peripheral; however the MSP430F5438A contains only the RTC_A peripheral on board. Could you please look into this and let me know about your specific setup?
Best regards,
Matt
Hi
Hello,
1) The RTC peripheral operates properly within the allowable voltage supply range of the device (1.8V - 3.6V)
2) The Reset pin going low triggers a brownout reset (BOR) which then causes the RTC register values to switch back to their default reset values as given in the user's guide Section 22.3.
3) Section 5.5 of the datasheet shows current consumption in different low power modes. You can refer to the LPM3 w/ VLO spec to get a rough estimate of the RTC current consumption. For example with a 3V supply at 25C and the device running in LPM3 with RTC enabled, the current consumption ranges from 1.2uA to 1.4uA.
Best regards,
Matt
**Attention** This is a public forum