Part Number: MSP430F5529
Other Parts Discussed in Thread: MSP-TS430PN80USB, , MSP-FET
Hello,
Using MSP-TS430PN80USB and BSL_USB_GUI.exe,
I am testing the USB BSL, but the USB is not recognized.
This board has MSP430F5529 rev c.
In addition, I checked the condition of PUR. When I press the BSL button of S3
I confirmed that it would be HIGH.
In addition, the following were confirmed.
The USB cable is connected while pressing the BSL button of S3.
In addition, PC uses windows10.
The jumper settings of the board are as follows.
JP1: short
JP3: internal
JP4: open
Since the device can be programmed with MSP-FET, it is determined that it is not broken.
What can happen if USB is not recognized?
Best regards,
DDdoor