Other Parts Discussed in Thread: MSP430FR6922
Hello,
I have a question regarding accessing hardware revision information from the MSP430F2617 devices.
I need to detect via uC software that the application is running on either the MSP430F2617TPM (64-PIN LQFP) or the MSP430F2617TZQW (113-PIN BGA)
Therefore if the uC software detects the BGA device then we can use PORTS 7 and 8.
Some of the MSP430 devices contain Hardware revision information stored in the Tag-Length Value (TLV) structures. For example the MSP430FR6922 contains Hardware revision and Die Record information.
Is there someway (other than using an external pull-up/pull-down resistor) to detect the MSP430F2617TPM and MSP430F2617TZQW devices using uC software ?
Is there Hardware revision information available to the CPU for both of these devices ?
Hoping you can assist me with this matter.
Kind Regards
Brendan