Tool/software: Code Composer Studio
HEY,
i am looking for a simple uart receiver program for studying. can anyone help me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
HEY,
i am looking for a simple uart receiver program for studying. can anyone help me?
I suggest you start with Example msp430g2xx3_uscia0_uart_01_115k.c (or similar) here:
http://dev.ti.com/tirex/explore/node?node=ALFfIDtjUH-HwRytz.WJPQ__IOGqZri__LATEST
The Echo part is in the ISR, where you see UCA0TXBUF=UCA0RXBUF. Replace that with code to do what you want.
I'm not sure I understand. Are you seeing data at your PC even if you don't type anything? Have you changed anything in the program?
If you don't want to use interrupts, you can poll for receive data in main().
1) Remove the line referring to UCA0RXIE
2) In main() insert a polling loop something like:
while (!(IFG2 & UCA0RXIFG)) /*EMPTY*/; // spin until Rx data appears RxByte = UCA0RXBUF; // Capture Rx data
Polling for Rx data is uncommon since in most applications it's unpredictable when the Rx data will arrive.
If you can tell us your overall goal, we can guide you a little better.
[Edit: Fixed code -- wrong MCU.]
I'm not quite sure I understand what you want to do.
The Example I mentioned above (unchanged) does what I think you're describing -- you connect the USB ("backchannel UART) to a terminal emulator on a PC, and whatever you type is echoed back to you. In between characters, it runs whatever code is in main (right now that isn't much, but you can add things).This is fairly cumbersome to accomplish without interrupts.
**Attention** This is a public forum