Hello,
I'm a bit of a newbie when it comes to the MSP430 family, and I have a hopefully easy question to answer. I'm using an MSP430FR5969 launchpad kit, and I need to configure the RTC to work in LPM3.5 using the VLO instead of a watch crystal. I can see in the datasheet that this is supposed to be possible, but I can't see how to configure the device that way. My first guess would be to assign the VLO as the source for ACLK, but that gets shutdown in LMP3.5.
Could someone point me in the right direction? I'd really appreciate it.