I tried to replace the launchpad for my MSP432P401R so I order some at Mouser. Unfortunately, the launchpads that I got are not 100% compatible with the initial launchpad MSP432P401R that I initially got with my robot TI-RSLK-MAX (J5 and another bank on the JTAG section are not populated and so, fail to connect with the robot chassis). The robot is OK, it is just the launchpad which seems to have entered into an autistic state, so it is just the launchpad which need to be replaced.
It there a different part ID that I should use to obtain a launchpad identical to the one which come with the robot? (instead of the ... standard ? ... one)