This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AFE4490SPO2EVM: Error: No USB FET was found when debugging Firmware of AFE4490

Part Number: AFE4490SPO2EVM
Other Parts Discussed in Thread: MSP430F5529, UNIFLASH

Tool/software: Code Composer Studio

Hi,
I installed the drivers of AFE4490SPO2EVM on the Windows 10 successfully (in the COM port list, I see AFE44xx... as the name of the COM port).

I can also communicate with the board using the GUI software to send the commands and receive the SPO2 data.

I also build its firmware in CCS successfully with no errors.

However, when I try to flash the newly-built firmware on the MCU board (MSP430F5529), I receive the error that says "Error initializing emulator: No USB FET was found".

The uniFlash software couldn't connect to the usb either.

**Attention** This is a public forum