Part Number: MSP430G2553
Hello all,
I need to write code which counts up/down and blinks led in order as shown in table.
UP MODE (1-2-...-7-0-1-...) / DOWN MODE (7-6-5-....-0-7..)
The count mode is required to be toggled by a switch connected to the pin P1.5. Between each count, specific amount of delay must be configured using TIMERA.
I wrote a code to count up but how can I toggle the count mode?
Here is my code :
#include<msp430.h>
int counter=0;
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
P1DIR |= 0x04; // Set P1.2 to output direction
P1DIR |= 0x02; // Set P1.1 to output direction
P1DIR |= 0x01; // Set P1.0 to output direction
P1OUT |= 0X20; // Configure P1.5 as pull-up
P1OUT = P1OUT & ~BIT0; // ... When program starts turn off LED 1
P1OUT = P1OUT & ~BIT1; // ... When program starts turn off LED 2
P1OUT = P1OUT & ~BIT2; // ... When program starts turn off LED 3
BCSCTL1=CALBC1_1MHZ; //Callibrate the frequency of timer as 1 MHZ
DCOCTL=CALDCO_1MHZ; //Callibrate the frequency of timer as 1 MHZ
CCTL0=CCIE; //CCR0 interrupt enabled
TACTL = TASSEL_2 + ID_0 + MC_1; //Select SMCLK, SMCLK/1, Up Mode
CCR0 = 50000; //Set the period to 50000*(1/1Mhz)=50 miliseconds
_BIS_SR(LPM0_bits + GIE); // Global enable interrupt and low power mode 0 (SMCLK available)
}
//Timer A0 interrupt service routine
#pragma vector=TIMER0_A0_VECTOR
__interrupt void Timer_A(void)
{
counter++; //Increment counter for each press
switch((counter/20)%8) //...1 sec delay
{
case 1:
P1OUT = P1OUT | BIT0; // ... turn on LED 1
P1OUT = P1OUT & ~BIT1; // ... turn off LED 2
P1OUT = P1OUT & ~BIT2; // ... turn off LED 3
break;
case 2:
P1OUT = P1OUT & ~BIT0; // ... turn off LED 1
P1OUT = P1OUT | BIT1; // ... turn on LED 2
P1OUT = P1OUT & ~BIT2; // ... turn off LED 3
break;
case 3:
P1OUT = P1OUT | BIT0; // ... turn on LED 1
P1OUT = P1OUT | BIT1; // ... turn on LED 2
P1OUT = P1OUT & ~BIT2; // ... turn off LED 3
break;
case 4:
P1OUT = P1OUT & ~BIT0; // ... turn on LED 1
P1OUT = P1OUT & ~BIT1; // ... turn on LED 2
P1OUT = P1OUT | BIT2; // ... turn off LED 3
break;
case 5:
P1OUT = P1OUT | BIT0; // ... turn on LED 1
P1OUT = P1OUT & ~BIT1; // ... turn on LED 2
P1OUT = P1OUT | BIT2; // ... turn off LED 3
break;
case 6:
P1OUT = P1OUT & ~BIT0; // ... turn on LED 1
P1OUT = P1OUT | BIT1; // ... turn on LED 2
P1OUT = P1OUT | BIT2; // ... turn off LED 3
break;
case 7:
P1OUT = P1OUT | BIT0; // ... turn on LED 1
P1OUT = P1OUT | BIT1; // ... turn on LED 2
P1OUT = P1OUT | BIT2; // ... turn off LED 3
break;
default:
P1OUT = P1OUT & ~BIT0; // ... turn off LED 1
P1OUT = P1OUT & ~BIT1; // ... turn off LED 2
P1OUT = P1OUT & ~BIT2; // ... turn off LED 3
break;
}
}
Any advice would be appreciated.
Thanks and Regards,
-Can.