Part Number: MSP430F5437A
Hi,
We are doing segment erase in flash and after it is completed by checking busy bit, we are doing Byte-Word write, in data section .infoB.
We repeat the above 6 times and then giving a delay of 4 secs. During this delay of 4 secs it is consuming 10 mA and while erasing and writing it is consuming around 7 mA.
Is there any internal modules of MSP430 are switched off to execute Flash operation ? Please clarify what may be the reason for reduce in current consumption?
Thanks,
Ayyappan M