Hello,
I struggle on the actual pin names of the MSP-EXP432P401R. I have the attached sheet with a pin map which was delivered with the MSP. But for the GPIOs it always states GPIO (!). So from the User Guide I know for example for the GPIO output function there are GPIO_PORT_P1 to P11/PJ and GPIO_PIN0-15. So now I am confused about what pin actually is GPIO_PIN0 and which is the corresponding port. Could anybody please help?