Part Number: MSP430FR2433
Tool/software: Code Composer Studio
I am using all the examples but i can't get the uart to work what am i doing wrong do yhou know a uart that i can use i mean p;rogram for the uart
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR2433
Tool/software: Code Composer Studio
I am using all the examples but i can't get the uart to work what am i doing wrong do yhou know a uart that i can use i mean p;rogram for the uart
Hi khary,
You can refer to those example code :
http://dev.ti.com/tirex/explore/node?node=AI9..X0EukhFuJAwALofbA__IOGqZri__LATEST
Best Regards
Johnson
do you know how do i disconnect the debugger... for the msp430fr2433 launchpad
using this example i cant get it to pc echo ... the example you are saying to use... i think it is getting stuck in lpm3 mode
Hi khary,
Could you show your hardware connect?
This example code is normal, maybe there are some other error, Could you provide some details with this issue?
Best Regards
Johnson
ok i was able to get working using an esp32 to transmit signals to the art thanks for your help
Hi khary,
An eUSCI-A module can only work in one mode at a time (SPI or UART). Therefore, UART and SPI cannot be used at the same time.
There are two eUSCI-A in FR2433, you can work one in UART mode and the other in SPI mode.
Best Regards
Johnson
eUSCI_A1 and eUSCI_A0 seem to be the two registers I need to communicate with this chip for SPI and Uart simultaneously
**Attention** This is a public forum