This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/MSP430FR2433: BSL download to target board, get "connection time out error, check the connection"

Part Number: MSP430FR2433


Tool/software: TI C/C++ Compiler

Dears,

    we use simulator to download firmware to MSP430FR2433 reference board. get "receive timeout, make sure connection is corrected".

    The connection to MSP430FR2433 reference board listed belows

    1:BSL transmit connected to P1.4

    2:BSL receive connected to P1.5

    3:BSL TCK    connected to SBWTCK

    4:BSL RST   connected to SBWTDIO/NMI/RST

    5:VCC/GOUND connected OK

    what's the problem's root cause?

thanks a lot and best regards

yuanxi.wang 

  • Can you confirm (using oscilloscope or logic probe) you are following the hardware BSL invocation timing on P1.4 and P1.5 shown in section 3.3.2 of the MSP430 FRAM BSL guide?

    Also, take a look at this list of things to check.

  • Hello,

    I haven’t heard from you for a couple of days now, so I’m assuming you were able to resolve your issue.
    If this isn’t the case, please click the "This did NOT resolve my issue" button and reply to this thread with more information.
    If this thread locks, please click the "Ask a related question" button and in the new thread describe the current status of your issue and any additional details you may have to assist us in helping to solve your issues.

**Attention** This is a public forum