This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2433: ADC sampling response

Part Number: MSP430FR2433


Has anyone used the 10 bit ADC at higher sampling frequencies? Would like to know if the response is linear at higher frequencies. 

  • Hi Kunal,

    It seems that the linearity of the value sampled by the ADC is not very related to the sampling frequency.

    Maybe you can do some test in 10 bit ADC mode.

    Best Regards

    Johnson

  • It seems some users of esp32 have pointed out that it doesn't pick up high audio frequencies faithfully. Just wanted to know cause I'll be using the msp430 for audio sampling around 80ksps

  • Hi Kunal,

    I will test the linearity of the value sampled when this module run in 80kps and go back update.

    Best Regards

    Johnson

  • Hi kunal,

    I do some test and post some data from my side as your reference :

    Test environment :

    VREF : 3.3V

    ADC : 10bit

    speed : 80kps

    Voltage 0.6 0.7 0.8 0.9 1 1.1 1.2 1.3 1.4 1.5 1.6 1.7 1.8 1.9 2 2.1 2.2 2.3 2.4 2.5 2.6 2.7 2.8 2.9 3
    ADC Value 186 215 249 277 309 344 373 405 435 465 500 529 561 592 619 651 684 716 745 779 809 840 869 901 935

    The test date show the linearity of the value is well, I do not found any problem.

    Best Regards

    Johnson

  • Hey Johnson, can you share the exact code you used?

  • There are my test code as your reference :

    #include <msp430.h>
    
    void Software_Trim();                       // Software Trim to get the best DCOFTRIM value
    #define MCLK_FREQ_MHZ 8                     // MCLK = 8MHz
    unsigned int adc_value = 0;
    
    int main(void)
    {
        WDTCTL = WDTPW | WDTHOLD;                                 // Stop WDT
    
        // Configure GPIO
        P1DIR |= BIT0;                                            // Set P1.0 to output direction
        P1OUT &= ~BIT0;                                           // Clear P1.0
    
        // Configure ADC A1 pin
        SYSCFG2 |= ADCPCTL1;
    
        // Configure XT1 oscillator
        P2SEL0 |= BIT0 | BIT1;                                    // P2.0~P2.1: crystal pins
    
        // Disable the GPIO power-on default high-impedance mode to activate
        // previously configured port settings
        PM5CTL0 &= ~LOCKLPM5;
    
        __bis_SR_register(SCG0);                // disable FLL
        CSCTL3 |= SELREF__REFOCLK;              // Set REFO as FLL reference source
        CSCTL1 = DCOFTRIMEN | DCOFTRIM0 | DCOFTRIM1 | DCORSEL_3;// DCOFTRIM=3, DCO Range = 8MHz
        CSCTL2 = FLLD_0 + 243;                  // DCODIV = 8MHz
        __delay_cycles(3);
        __bic_SR_register(SCG0);                // enable FLL
        Software_Trim();                        // Software Trim to get the best DCOFTRIM value
    
        CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK; // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz
                                                   // default DCODIV as MCLK and SMCLK source
    
        // Configure ADC
        ADCCTL0 |= ADCON | ADCMSC;                                // ADCON
        ADCCTL1 |= ADCSHS_2 | ADCCONSEQ_2;                        // repeat single channel; TA1.1 trig sample start
        ADCCTL2 |= ADCRES;                                        // 10-bit conversion results
        ADCMCTL0 |= ADCINCH_1 | ADCSREF_0;                        // A1 ADC input select; Vref=1.5V
        ADCIE |= ADCIE0;                                          // Enable ADC conv complete interrupt
    
        // Configure reference
        PMMCTL0_H = PMMPW_H;                                      // Unlock the PMM registers
        PMMCTL2 |= INTREFEN;                                      // Enable internal reference
        __delay_cycles(400);                                      // Delay for reference settling
    
        ADCCTL0 |= ADCENC;                                        // ADC Enable
    
    
        // ADC conversion trigger signal - TimerA1.1 (80KHz ON-period)
        TA1CCR0 = 100-1;                                         // PWM Period
        TA1CCR1 = 50-1;                                          // TA1.1 ADC trigger
        TA1CCTL1 = OUTMOD_4;                                      // TA1CCR0 toggle
        TA1CTL = TASSEL__SMCLK | MC_1 | TACLR;                     // ACLK, up mode
    
        __bis_SR_register(LPM0_bits | GIE);                       // Enter LPM3 w/ interrupts
    }
    
    // ADC interrupt service routine
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=ADC_VECTOR
    __interrupt void ADC_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(ADC_VECTOR))) ADC_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
        switch(__even_in_range(ADCIV,ADCIV_ADCIFG))
        {
            case ADCIV_NONE:
                break;
            case ADCIV_ADCOVIFG:
                break;
            case ADCIV_ADCTOVIFG:
                break;
            case ADCIV_ADCHIIFG:
                break;
            case ADCIV_ADCLOIFG:
                break;
            case ADCIV_ADCINIFG:
                break;
            case ADCIV_ADCIFG:
                adc_value = ADCMEM0;
    //            if (ADCMEM0 < 0x155)                             // ADCMEM = A0 < 0.5V?
    //                P1OUT &= ~BIT0;                              // Clear P1.0 LED off
    //            else
    //                P1OUT |= BIT0;                               // Set P1.0 LED on
                ADCIFG = 0;
                break;                                           // Clear CPUOFF bit from 0(SR)
            default:
                break;
        }
    }
    
    void Software_Trim()
    {
        unsigned int oldDcoTap = 0xffff;
        unsigned int newDcoTap = 0xffff;
        unsigned int newDcoDelta = 0xffff;
        unsigned int bestDcoDelta = 0xffff;
        unsigned int csCtl0Copy = 0;
        unsigned int csCtl1Copy = 0;
        unsigned int csCtl0Read = 0;
        unsigned int csCtl1Read = 0;
        unsigned int dcoFreqTrim = 3;
        unsigned char endLoop = 0;
    
        do
        {
            CSCTL0 = 0x100;                         // DCO Tap = 256
            do
            {
                CSCTL7 &= ~DCOFFG;                  // Clear DCO fault flag
            }while (CSCTL7 & DCOFFG);               // Test DCO fault flag
    
            __delay_cycles((unsigned int)3000 * MCLK_FREQ_MHZ);// Wait FLL lock status (FLLUNLOCK) to be stable
                                                               // Suggest to wait 24 cycles of divided FLL reference clock
            while((CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)) && ((CSCTL7 & DCOFFG) == 0));
    
            csCtl0Read = CSCTL0;                   // Read CSCTL0
            csCtl1Read = CSCTL1;                   // Read CSCTL1
    
            oldDcoTap = newDcoTap;                 // Record DCOTAP value of last time
            newDcoTap = csCtl0Read & 0x01ff;       // Get DCOTAP value of this time
            dcoFreqTrim = (csCtl1Read & 0x0070)>>4;// Get DCOFTRIM value
    
            if(newDcoTap < 256)                    // DCOTAP < 256
            {
                newDcoDelta = 256 - newDcoTap;     // Delta value between DCPTAP and 256
                if((oldDcoTap != 0xffff) && (oldDcoTap >= 256)) // DCOTAP cross 256
                    endLoop = 1;                   // Stop while loop
                else
                {
                    dcoFreqTrim--;
                    CSCTL1 = (csCtl1Read & (~(DCOFTRIM0+DCOFTRIM1+DCOFTRIM2))) | (dcoFreqTrim<<4);
                }
            }
            else                                   // DCOTAP >= 256
            {
                newDcoDelta = newDcoTap - 256;     // Delta value between DCPTAP and 256
                if(oldDcoTap < 256)                // DCOTAP cross 256
                    endLoop = 1;                   // Stop while loop
                else
                {
                    dcoFreqTrim++;
                    CSCTL1 = (csCtl1Read & (~(DCOFTRIM0+DCOFTRIM1+DCOFTRIM2))) | (dcoFreqTrim<<4);
                }
            }
    
            if(newDcoDelta < bestDcoDelta)         // Record DCOTAP closest to 256
            {
                csCtl0Copy = csCtl0Read;
                csCtl1Copy = csCtl1Read;
                bestDcoDelta = newDcoDelta;
            }
    
        }while(endLoop == 0);                      // Poll until endLoop == 1
    
        CSCTL0 = csCtl0Copy;                       // Reload locked DCOTAP
        CSCTL1 = csCtl1Copy;                       // Reload locked DCOFTRIM
        while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // Poll until FLL is locked
    }
    

    Best Regards

    Johnson

**Attention** This is a public forum