Part Number: MSP430FR2676
Would it be possible to use UART pins of the device as LIN instead?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR2676
Would it be possible to use UART pins of the device as LIN instead?
Hi,
as far as I know you need a UART which supports automatic baud rate detection to support LIN right. At least this is what I read from following 2 links:

See also FR2676 users guide chapter 22.3.4. for further information there also LIN is mentioned.
So simple answer yes LIN is possible with FR2676.
Thanks Dietmar.
I read in the pres. you provided (slide 30), that:
So it would mean that a LIN driver IC is still required, right?
Bart,
please take a look to the LIN specification:
In chapter 6.5.4ELECTRICAL DC PARAMETERS you can see that voltage specifications. The voltage spec of LIN does not match the max 3.6V therefore an external LIN bus driver is required.
Some examples can be found here also the datasheets of some parts has some implementation proposals:
**Attention** This is a public forum