Part Number: MSP430FR2522
Hi Team,
My customer now want to select MSP430 to detect the capacitive touch buttons on the car, which need to meet at least the operating temperature of -40-100, do you have a suitable recommendation?
The specific application scenario is a main MCU + an auxiliary MCU, the main MCU is responsible for CAN \ LIN communication, and the auxiliary MCU (MSP430) is responsible for the detection of capacitive buttons. If there is a single-chip MCU that can meet the two functions better.
Could you please give some guidance? Thanks!