This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6047: Can the Meter Bus Wireless Serial Library be used for a Wired Meter Bus setup?

Part Number: MSP430FR6047
Other Parts Discussed in Thread: MSP430FR6989, TSS721A,

Hello,

I am working on a design that needs a wired Meter Bus communication and using the TSS721A as the interface IC for the slave device. I saw in another post that TI has a Wireless MeterBus Serial Library but can this be modified for a wired connection? and is it compatible with the MSP430FR6989 micro? Also there is a TI MeterBus to RS485 Data Collector example called (below), Is this using the same library or is there another one available? and can it be used to read and respond to MeterBus requests?

TIDM-1005 Data Collector With M-Bus and RS485 protocol Conversion Reference Design

Thks!

Mark

**Attention** This is a public forum