Part Number: MSP430F6747A
Hi everybody,
I would like to use http://www.ti.com/tool/download/MSP430-ENERGY-MEASUREMENT
now about if this toolkit:
- Can perform for higher frequencies, such as 5kHz, which is similar to 50/60Hz?
- Does it supports an AC signal which has an offset, for example an AC wave 100 ~ 300VAC which rides on 200VAC (which has no 0 point crossing).
best regards
Carlo