Part Number: MSP430FR5870
MSP430 team,
Can you help with some more details about ADC67? We have a customer affected by this, and it would help to know:
1. Approximately what percentage of devices are affected by the errata?
2. The calibration data is listed in the errata as being "invalid" and "incorrect". Can you say if the values are off by some percentage, or are they as good as random numbers?
Here is the errata description:
The ADC12 reference temperature sensor calibration data stored in the TLV data structure (0x1A1A - 0x1A25) can be incorrect depending on the production lot trace code. As a result the temperature measurement when using these data can be wrong. Devices with lot trace code > 88XXXXX are not affected by this issue.
Thanks,
Darren