Part Number: MSP430F67451A
Hi community member,
Is there anything to consider when using both the ADC10_A and SD24_B built into the MSP430F67451A at the same time?
Best Regards,
O.H
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F67451A
Hi community member,
Is there anything to consider when using both the ADC10_A and SD24_B built into the MSP430F67451A at the same time?
Best Regards,
O.H
Hi O.H,
SD24 is for energy measurement and power monitoring
10-Bit 200-ksps SAR ADC With Six External Channels and Two Internal Channels, Including Supply and Temperature Sensor Measurement
Thanks!
Hi Xiaodong Li,
Thank you for your reply.
Does it mean that I can use both at the same time?
Best Regards,
O.H
**Attention** This is a public forum