Part Number: EVM430-FR6047
Hi TI-Team,
I have a question regarding the payload structure of the messages for the two commands:
- Command 0x97 (Request Delta ToF, Abs ToF and Volume Flow data)
- Command 0x98 (Request UPS and DNS captures)
I can receive the payload after sending the reqeuest very well.
But I did not yet understand the structure of the message payload completely.
How can I read/convert the actual value (float/int) from the payload?
Two examples:
A) Command 0x97 (Request Delta ToF, Abs ToF and Volume Flow data)
1.
SEND command 0x97 to EVM:
2.
RECEIVE msg 0xB3 from EVM:
???-> how to convert payload now to measuring value???
Documentation says float data type Byte[3](LSB), Byte[6](MSB).
So is the float data:
3e-ec-c4-00 = 0.462432861 (float little endian DCBA) ?
----------------------------------------------------------------------------------------------------
B) Command 0x98 (Request UPS and DNS captures)
SEND 'request command' to EVM:
RECEIVE 'start command' from EVM:
RECEIVE 'payload packages from EVM: 
Documentation says int16_t (-32768,32767). So I guess two bytes = one int16_t. But which bytes to read first, and which one is MSB/LSB?
Do I start with package one, payload 0/payload1 and end with package 6 payload 55/56?
So in this case:
first adc capture value: 08-00 = 2048 (signed int big endian AB)
last adc capture value: 01-00 = 256 (signed int big endian AB) ?
Thank you for your help
Best regards
Lucio