Part Number: MSP430FR2311
Other Parts Discussed in Thread: MSP430WARE
Hi TI Team,
I am looking sample code implementation of ADC raw data to milli volt code conversion using msp430fr2311.
Any ideas?
Regards,
Walter
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR2311
Other Parts Discussed in Thread: MSP430WARE
Hi TI Team,
I am looking sample code implementation of ADC raw data to milli volt code conversion using msp430fr2311.
Any ideas?
Regards,
Walter
Hi Walter,
When converting from ADC data to an equivalent input voltage, you'll need to know the reference voltage (VREF) and the ADC resolution (n). For example, the minimum LSB size in Volts = VREF / (2^n) = 1.5 V / (2^10) = 1.465 mV. Keep in mind that VREF can be different (e.g. 1.5 V or DVCC) depending on the device and/or settings. Also, a lower VREF for the same ADC resolution (n) results in a lower LSB size, but the input range is lower and limited to VREF. Check out Section 2.1.2 in the Designing With MSP430FR58xx/FR59xx/68xx/69xx ADC app note.
The 'msp430fr231x_adc10_05.c' code example should be what you're looking for. You can find it inside CCS by going to TI Resource Explorer > Software > MSP430Ware > Devices > MSP430FR2XX_4XX > MSP430FR2311 > Peripheral Examples > Register Level. You may need to install MSP430Ware in order to import the project into your CCS workspace. I've copied it below for your reference.
msp430fr231x_adc10_05.c
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2014, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430FR231x Demo - ADC, Lo_Batt, Set P1.0 if AVcc < 2.50V
//
// Description: A single sample is made on A13 (Vref) with reference set to
// DVCC. Software sets ADC10SC to start sample and conversion
// - ADC10SC automatically cleared at EOC. Once conversion is completed, the
// following equation is used to calculate DVCC = (1023 * 1.5) / adcResult.
// if DVCC is < 2.5V, P1.0 set indicating a lo_Batt condition, else reset.
//
// MSP430FR2311
// -----------------
// /|\| XIN|-
// | | |
// --|RST XOUT|-
// | |
// |A13 (Vref) P1.0|-->LED
//
// Darren Lu
// Texas Instruments Inc.
// July 2015
// Built with IAR Embedded Workbench v6.30 & Code Composer Studio v6.1
//******************************************************************************
#include <msp430.h>
unsigned int adcResult; // Temporarily stores the ADC value
// that was read from ADCMEM0
int main(void)
{
volatile unsigned long dvccValue; // Calculated DVCC value
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
P1DIR |= BIT0; // Set P1.0 to output direction
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Configure ADC10
ADCCTL0 &= ~ADCENC; // Disable ADC
ADCCTL0 = ADCSHT_2 | ADCON; // ADCON, S&H=16 ADC clks
ADCCTL1 = ADCSHP; // ADCCLK = MODOSC; sampling timer
ADCCTL2 = ADCRES; // 10-bit conversion results
ADCIE = ADCIE0; // Enable ADC conv complete interrupt
ADCMCTL0 = ADCINCH_13 | ADCSREF_0; // A13 ADC input select = 1.5V Ref
// Vref = DVCC
// Configure reference module located in the PMM
PMMCTL0_H = PMMPW_H; // Unlock the PMM registers
PMMCTL2 |= INTREFEN; // Enable internal reference
while(!(PMMCTL2 & REFGENRDY)); // Poll till internal reference settles
while(1)
{
ADCCTL0 |= ADCENC | ADCSC; // Sampling and conversion start
__bis_SR_register(LPM0_bits | GIE); // Enter LPM0, ADC_ISR will force exit
__no_operation(); // For debug only
// To calculate DVCC, the following equation is used
// DVCC = (1023 * 1.5) / adcResult
// The following equation is modified to use only integers instead
// of using float. All results needs to be divided by 100 to obtain
// the final value.
// DVCC = (1023 * 150) / adcResult
dvccValue = ((unsigned long)1023 * (unsigned long)150) / (unsigned long) (adcResult);
if (dvccValue < 250) // DVCC < 2.50V?
P1OUT |= BIT0; // Set P1.0 LED on
else
P1OUT &= ~BIT0; // Clear P1.0 LED off
}
}
// ADC interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=ADC_VECTOR
__interrupt void ADC_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC_VECTOR))) ADC_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(ADCIV, ADCIV_ADCIFG))
{
case ADCIV_NONE:
break;
case ADCIV_ADCOVIFG:
break;
case ADCIV_ADCTOVIFG:
break;
case ADCIV_ADCHIIFG:
break;
case ADCIV_ADCLOIFG:
break;
case ADCIV_ADCINIFG:
break;
case ADCIV_ADCIFG:
adcResult = ADCMEM0; // Read ADC memory
__bic_SR_register_on_exit(LPM0_bits);// Exit from LPM
break;
default:
break;
}
}
Regards,
James
Hi james,
This is one is what I need precisely because I was trying to detect low battery level.
If say, I will not use 1.5 reference and use only DVCC as reference. Will it still work if I am measuring DVCC but it is also the reference in this case?
Regards,
Walter
Hi Walter :
If you want to monitor the battery voltage you need to use internal 1.5 V reference. Because a Battery system the DVCC is battery voltage, so the DVCC will decrese as time pass.
Regards;
Marshall Wu
Hi Marshall,
I see it can work using 1.5V reference using AD13.
I want to know the delay in reference settling like the one below. I cannot find in data sheet or user guide.
// Configure reference
PMMCTL0_H = PMMPW_H; // Unlock the PMM registers
PMMCTL2 |= INTREFEN; // Enable internal reference
__delay_cycles(400); // Delay for reference settling??
How did they get the optimum value.
Regards,
Walter
Hi Walter,
The reference settling time should be provided in the datasheet. Then, depending on your CPU clock speed, you can adjust the number of cycles to achieve that settling time delay.
Regards,
James
Hi Team,
I am talking only about the optimum value for the 1.5V reference to settle in msp430fr2311 device.
I cannot find in specs.
Regards,
Walter
Hi Walter,
According to Section 21.2.3.1 Internal Reference Low-Power Features in the MSP430FR4xx and MSP430FR2xx family user's guide, the settling time is less than or equal to 30 us.
Regards,
James
If you have any other questions, please post them in a new thread. I think we've resolved your original question. Thanks.
Regards,
James
**Attention** This is a public forum