Other Parts Discussed in Thread: MSP430F2617
I would like to be able to quickly program the MSP430 with FET-Pro430 by Elprotronics. The issue is that when I try to program through FET-Pro430 using the *.hex file output from CCSV4 nothing happens. It says that it has programmed with all checks passed, but then the MSP doesn't run. Whereas when I use debug in CCSV4 to program the MSP it runs.
Are there some settings in either CCSV4 or FET-Pro430 that need to be changed?
Installation:
- Windows 7 x64
- CCS v4.2.1.00004
- MSP-FET430 UIF 'V1.4a' Firmware 2.04.07.001
- MSP430F2617
Thanks,
Lucas