This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430I2021: About Designing Around RST Pins

Part Number: MSP430I2021

Hi experts,

Circuit around RST using MSP430I2021 is performing unexpected operation due to the effect of noise.

Could you tell me about the following items?
1)Is there an internal circuit for the RST pin of the MSP430I2021?
(It is not a block diagram like the one in the user's guide "Figure 1-1", but rather a circuit for connecting the RST pin to the internal core.)

2)The MSP430I2021 does not have an internal pull-up/down resistor, right?

3)Is it okay to set the pull-up resistance of the following circuit to 100ohms?

Currently, the circuit shown in the figure below is constructed, but when noise is applied, the circuit is reset.

Changing the resistance to 100ohms will not be affected by noise.
(Changing the resistance to 510ohms will be affected by noise.)

Best Regards,
O.H

**Attention** This is a public forum