This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401V: Can't get UART DMA working

Part Number: MSP432P401V


I am converting existing and generally-working UART RX code at 115200 to DMA because an occasional character is dropped. I disabled the currently-used EUSCI_A_UART_RECEIVE_INTERRUPT and wrote the following code to implement DMA. DMA_INT2_IRQHandler() is not being called. I'm also unsure of what code needs to be inside this interrupt handler to make sure DMA is re-enabled for the next character. Can anyone tell me what is wrong with this code? Thanks.

/* DMA Control Table */
#pragma data_alignment=1024
uint8_t controlTable[1024];

static void DMA_Enable( void )
{
    /* Configuring DMA module */

    MAP_DMA_enableModule();

    MAP_DMA_setControlBase(controlTable);

    /* Assigning Channel 3 to EUSCIA1RX*/
    MAP_DMA_assignChannel(DMA_CH3_EUSCIA1RX);

    /* Disabling channel attributes of alternate DMA channel which will not be used in the basic DMA mode */
//    MAP_DMA_disableChannelAttribute(DMA_CH3_EUSCIA1RX, UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST | UDMA_ATTR_REQMASK);

    /* Setting control parameters: 'UDMA_SIZE_8' and 'UDMA_SRC_INC_8' are selected coz UART TX/RX data buffer size limited to one character */
    // primary channel
    MAP_DMA_setChannelControl(DMA_CH3_EUSCIA1RX | UDMA_PRI_SELECT,  UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 | UDMA_ARB_1);

    /* Setting channel transfers */
    MAP_DMA_setChannelTransfer(DMA_CH3_EUSCIA1RX | UDMA_PRI_SELECT, UDMA_MODE_BASIC,
            (void*) MAP_UART_getReceiveBufferAddressForDMA(UART_IN_USE_BASE), s_RxBuffer, 10);

    /* Assigning interrupts */
    MAP_DMA_assignInterrupt(DMA_INT2, 3);
    MAP_Interrupt_setPriority( INT_DMA_INT2, 0x00 );
    MAP_Interrupt_enableInterrupt(INT_DMA_INT2);
    MAP_DMA_enableInterrupt(INT_DMA_INT2);

    /* Enable DMA channel */
    MAP_DMA_enableChannel(3);
}

void DMA_INT2_IRQHandler(void)
{
    MAP_DMA_setChannelTransfer(UDMA_PRI_SELECT | DMA_CH3_EUSCIA1RX,
            UDMA_MODE_BASIC,
            (void*)MAP_UART_getReceiveBufferAddressForDMA(UART_IN_USE_BASE), s_RxBuffer,
            10);

    // Reenable the DMA Rx Transfer
    MAP_DMA_enableChannel( 3 );
}

**Attention** This is a public forum