Part Number: MSP-EXP430FR5994
Other Parts Discussed in Thread: TUSB3410, BOOSTXL-AUDIO
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP-EXP430FR5994
Other Parts Discussed in Thread: TUSB3410, BOOSTXL-AUDIO
Hi,
Do you mean that you need transfer data to PC through UART? And what is the sampling rate for?
Best regards,
Cash Hao
Hi Basavaraj,
FR5994 does not have a dedicated USB module but you can use the UART to transfer data to the PC using RS232 interface via a simple hyperterminal.
If you do have a RS232 on you PC but only USB there alternative solutions. One is to use the TUSB3410 to implement a UART to USB bridge to you PC and you a virtual com port on your PC hyperterminal. Some more information can be found below.

You also can select another MSP device like F6638 or F5529 which comes with USB module implemented.
Hi Walther,
Thank you for the reply and details.
But the part I am referring to is MSP-EXP430FR5994 the Launchpad development platform, I am going to use along with
BOOSTXL-AUDIO Audio BoosterPack™ Plug-in Module, And I Need to take the Microphone samples directly to PC during development, debug phase .
Hence the sampling rate is mentioned. Is there a way to take it to PC , samples from microphone as we already have USB interface through eZ-FET hardware section on board MSP-EXP430FR5994 Launch pad.
Hope I am bit more clear now.
Kind regards
Basavaraj B M
Hi Walther,
Thank you for the details. Will check it out once the launchpad board in our hand, as it is still in transit and expected any moment.
Hopefully back channel UART should suffice , with 8K sampling rate.
kind regards
Basavaraj B M
**Attention** This is a public forum