Part Number: MSP430I2040
Hi,
We are using MSP430i2040 for measuring the differential analog input and found there is a difference of 0.67mV in the ADC result when we short the A+ and A- terminal which should result in 0mV as the difference will be zero.
I have attached the schematics and the sample code used for testing, please let us know the gain or any other missing configuration that required to be added in the code.
#include "msp430i2040.h"
unsigned int storeone;
void main(void) {
WDTCTL = WDTPW | WDTHOLD;
SD24CTL = SD24REFS;
SD24CCTL0 |= SD24SNGL | SD24DF;
SD24CCTL1 |= SD24SNGL | SD24DF;
__delay_cycles(3200); // Delay
__bis_SR_register(GIE);
while (1) {
SD24CCTL0 |= SD24SC;
while (!(SD24CCTL0 & SD24IFG))
;
storeone = SD24MEM0;
}
}