Hi,
Here is the code of pwm generation, but i want gradual increase in pwm and it should get out on LED connected to port 3.7, In code i have used external oscillator of 32KHz , what modifications should i do for that???? please help me :((
#include<msp430x21x2.h>
#include
#define
void timer_init();
pwmpr 511<intrinsics.h>
volatileunsigned int i;
void
main()
{ WDTCTL = WDTPW + WDTHOLD;
BCSCTL3 |= LFXT1S0;
// + LFXT1OF; // LFXT1S1 = 3-16Mhz BCSCTL1|=DIVA_3;
BCSCTL3|=XCAP_2;
do
{IFG1 &= ~OFIFG;
// Clear OSCFault flag
for (i = 0xFF; i > 0; i--);
// Time for flag to set
}
while (IFG1 & OFIFG);
// OSCFault flag still set?
BCSCTL2 |= SELM_3;
// MCLK = LFXT1 (safe)
P1DIR|=0X10; P2DIR|=0X02; P3DIR|=0X80; P1SEL|= 0X10; P2SEL|= 0X02; P3SEL|= 0X80; TA1CCR0 = pwmpr; TA1CCTL1 = OUTMOD_7;
// + CCIE; //TA1CCR1=start1; // + CM_2 + SCCI + SCS;
TA1CTL = TASSEL_1 + MC_1 + TAIE;
// + TACLR;+ TAIFG; + ID_3 ; ACLK, up
__bis_SR_register(GIE);
//_EINT(); CPU off
}
//**************************************************************
#pragma
vector= TIMER1_A1_VECTOR
__interrupt
void TIMER1_A1(void)
{
unsigned int j=50000;
if (TA1IV==0X0a)
TA1CCR1+=10;
{
do
j--;}
while (j!=0);
}
}