Part Number: EVM430-CAPMINI
Other Parts Discussed in Thread: CAPTIVATE-PGMR, , MSP-FET
Tool/software: Code Composer Studio
I want to know if I can develop on the EVM430-CAPMINI using the CAPTIVATE-PGMR.
The CAPMINI docs say: "To create user’s own code or demo, use the on-board Spy-bi-wire debug port."
The CAPTIVATE-PGMR has Spy-Bi-Wire Interface.
Seems I could set it up like this:
COMPUTER <---USB---> CAPTIVATE-PGMR<---SPY-bi-wire --->EVM430-CAPMINI
However, Section 2.3 of the CAPMINI docs (http://www.ti.com/lit/ug/slau784/slau784.pdf?ts=1590212413389
"You must use a hardware debug tool to program the MSPFR2512 MCU. The MSP-FET is a powerful
debug probe for application development and supports all MSP430 microcontrollers. The eZ-FET is a
powerful onboard emulator and is on LaunchPad™ development kits."