Part Number: MSP430F5419A
Tool/software: TI C/C++ Compiler
I am trying to make reader in pin 1.0 to read a trace of 8 bits.
Due the others uart port are not available i have to put this TX TTL device to comunicate via this pin.
To make this posible i configurate this pin to start read when generating a interruption and then read the trace of 8 bit.
The external device is configurated in 9600 bauds so the actual objective i have is read this pin every 20,75us, 8 times.
The problem i have is:
I tried to configurate a timer to read every 20,75 us but i thing the resolution is 1ms.
Do you know any solution to this problem?
I tried the function delay( ) but i think has the same resolution.
Thank you in advance.