This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5989: MSPFlasher verification error

Part Number: MSP430FR5989

I am currently working on the project and using IAR and MSP Flasher.

In our project we are using IPE and is password protected. When I flash using IAR the flashing along with verification succeeds , however with MSP flasher the verification fails.

Please find the output from MSP Flasher Below.

;

C:\ti\MSPFlasher_1.3.18>MSP430Flasher.exe -n MSP430FR5989 -m AUTO -e ERASE_ALL -w msp430.hex -v msp430.hex -z [VCC] -p 0xaaaa0b84ffffffff

* -----/|-------------------------------------------------------------------- *

*     / |__                                                                   *

*    /_   /   MSP Flasher v1.3.18                                             *

*      | /                                                                    *

* -----|/-------------------------------------------------------------------- *

*

* Evaluating triggers...done

* Checking for available FET debuggers:

* Found USB FET @ COM12 <- Selected

* Initializing interface @ COM12...done

* Checking firmware compatibility:

* FET firmware is up to date.

* Reading FW version...done

* Setting VCC to 3000 mV...done

* Accessing device...done

* Reading device information...done

* Loading file into device...done

* Verifying memory (msp430.hex)...

# Exit: 60

# ERROR: Verification error

* Starting target code execution...done

* Disconnecting from device...done

*

* ----------------------------------------------------------------------------

* Driver      : closed (EEM polling thread is already active)

* ----------------------------------------------------------------------------

*/

 

Can you please help me with the right command and how I can ensure that we don’t get verification error?

**Attention** This is a public forum