Part Number: MSP432P401R
Hi,
I am trying to communicate to a slave using MSP432 mC. I am able to transmit & receive data using the 'uart.c' library when I run the project (modified using the example file) without OS.
When I run the project (again modified from example file) with FreeRTOS OS, I can see that data is getting transmitting using UART, by looking at the registers. However, I don't receive any input back from the slave.
I am using simple hex codes to transmit & receive through uart. Also, when I use FreeRTOS, the sample file is linked to UART.h, whereas without OS it is linked to another library uart.h.
Kindly help me understand the difference & rectify the issue. I suspect, it could be due to Baud rate differences. Howver, I am not able to figure out.
Regards,
Navin