This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6972: reset use

Part Number: MSP430FR6972

When MSP430FR6972 is used, there are the following phenomena: 1) When the power is close to the reset pin, 430 will go offline to reset pin work during work, resulting in MCU reset;2) When THE NB module is close to the power source and the reset pin, when NB network is connected, the off-line reset pin work will occasionally occur, leading to MCU reset.How to solve the above problems? What IC can be added to the reset pin line?

**Attention** This is a public forum