Part Number: MSP430FR6972
When MSP430FR6972 is used, there are the following phenomena: 1) When the power is close to the reset pin, 430 will go offline to reset pin work during work, resulting in MCU reset;2) When THE NB module is close to the power source and the reset pin, when NB network is connected, the off-line reset pin work will occasionally occur, leading to MCU reset.How to solve the above problems? What IC can be added to the reset pin line?