This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6047: Connect the EVM to Tida-01486

Part Number: EVM430-FR6047


Hello,

I´m not sure how to clamp the EVM to the Tida Board. Do I have to split the in- and output-channels from the EVM, remove R16/17 and C11/12? Or leave it and clamp them between the two boards?

My next Question is: I want to use only one pair of transducers. In this case I don´t need any multiplexers from the Tida reference-design, or  am I wrong?

Thanks for supporting me.

Frank

**Attention** This is a public forum