This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR4133: ccs/msp430

Part Number: MSP430FR4133


Tool/software: Code Composer Studio

I just acquired one of these new Launchpad msp430fr4133. I tried to work with it, Upon trying to access the device, I got a notice saying the Launchpad firmware needs updating. I clicked on the "Update" button and both red/green LEDs on the ez-FET came on and the "Out-of-the-box" project  stopped running. It just sat there until I noticed that there was an error in communication with the device appearing in the Console window and it stopped dead. Now the Launchpad is not recognized neither in the Linux nor in the widow. In the ccs window DEBUG show "TI MSP430 USB1/MSP430(Disconnected : unknown ), i have just purchase this kit and did not even run first application, please help me how can i overcome this problem.

  • Hi Asim,

    Usually, the debugger section can recover, if the FW update failed. Thus if you could try it with another PC or after restoration of the initial one, you might be able to recover the LP. But of course it might happen, that you will not be able to recover the tool. It this case, you can return this LP back and get a new one. Sorry for the inconvenience.

**Attention** This is a public forum