Other Parts Discussed in Thread: TPD1E10B06
Hello,
In MSP430 datasheet, Table 5-23 states a maximum value for all electrodes capacitance:
Questions:
1- I have 16 electrodes each connected to a pin, is this 300pF the sum of all of them or for each block? (i.e. each electrode of the 16 will have a max value of 300pF/16 = 18pF or 300 each)?
2- The frequency of the captivate output signal is 4-16MHz, is there a way to decrease it further or not?
Thanks