This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430F5529LP: Compile Error, Library for Energia

Part Number: MSP-EXP430F5529LP
Other Parts Discussed in Thread: ENERGIA,

I am using energia to code the board but when i tried to import arduino library i get these error when compiling. Please can you help me to sort these compile errors?

 

Energia: 1.8.11E23 (Windows 10), Board: "MSP-EXP430F5529LP"

In file included from C:\........\Energia\libraries\tic-arduino-master\examples\I2CMulti\I2CMulti.ino:18:0:

C:\........\Energia\libraries\tic-arduino-master/Tic.h:17:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:44:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:65:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:95:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:109:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:120:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:134:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:162:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\libraries\tic-arduino-master/Tic.h:182:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:193:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:209:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:220:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:229:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:241:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:250:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:274:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:286:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:296:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1281:24: error: ISO C++ forbids initialization of member '_lastError' [-fpermissive]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1281:24: error: making '_lastError' static [-fpermissive]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1281:24: error: ISO C++ forbids in-class initialization of non-const static member '_lastError'

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1357:24: error: 'TicProduct' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1357:36: error: ISO C++ forbids initialization of member 'product' [-fpermissive]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1357:36: error: making 'product' static [-fpermissive]

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1357:36: error: ISO C++ forbids in-class initialization of non-const static member 'product'

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setTargetPosition(int32_t)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:347:16: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setTargetVelocity(int32_t)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:367:16: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::haltAndSetPosition(int32_t)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:388:16: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::haltAndHold()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:409:18: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::goHomeReverse()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:419:15: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::goHomeForward()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:429:15: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::resetCommandTimeout()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:442:18: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::deenergize()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:466:18: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::energize()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:481:18: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::exitSafeStart()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:496:18: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::enterSafeStart()':

C:\........\\Energia\libraries\tic-arduino-master/Tic.h:516:18: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::reset()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:530:18: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::clearDriverError()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:548:18: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setMaxSpeed(uint32_t)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:564:16: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setStartingSpeed(uint32_t)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:580:16: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setMaxAccel(uint32_t)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:597:16: error: 'TicCommand' is not a class or namespace
C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setMaxDecel(uint32_t)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:614:16: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setStepMode(TicStepMode)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:631:15: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setDecayMode(TicDecayMode)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:668:15: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setAgcMode(TicAgcMode)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:678:15: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setAgcBottomCurrentLimit(TicAgcBottomCurrentLimit)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:688:15: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setAgcCurrentBoostSteps(TicAgcCurrentBoostSteps)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:698:15: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setAgcFrequencyLimit(TicAgcFrequencyLimit)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:708:15: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicOperationState TicBase::getOperationState()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:726:39: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'bool TicBase::getEnergized()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:733:20: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h:734:16: error: 'TicMiscFlags1' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'bool TicBase::getPositionUncertain()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:744:20: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h:745:16: error: 'TicMiscFlags1' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'bool TicBase::getForwardLimitActive()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:751:20: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h:752:16: error: 'TicMiscFlags1' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'bool TicBase::getReverseLimitActive()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:758:20: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h:759:16: error: 'TicMiscFlags1' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'bool TicBase::getHomingActive()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:765:20: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h:766:16: error: 'TicMiscFlags1' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getErrorStatus()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:784:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getErrorsOccurred()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:807:16: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h:808:7: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicPlanningMode TicBase::getPlanningMode()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:827:37: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'int32_t TicBase::getTargetPosition()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:838:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'int32_t TicBase::getTargetVelocity()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:849:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getMaxSpeed()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:860:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getStartingSpeed()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:876:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getMaxAccel()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:892:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getMaxDecel()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:908:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'int32_t TicBase::getCurrentPosition()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:923:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'int32_t TicBase::getCurrentVelocity()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:939:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getActingTargetPosition()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:951:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getTimeSinceLastStep()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:964:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicReset TicBase::getDeviceReset()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:980:30: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getVinVoltage()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:991:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getUpTime()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1005:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'int32_t TicBase::getEncoderPosition()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1016:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getRCPulseWidth()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1034:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getAnalogReading(TicPin)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1054:22: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'bool TicBase::getDigitalReading(TicPin)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1071:32: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicPinState TicBase::getPinState(TicPin)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1090:30: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicStepMode TicBase::getStepMode()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1105:33: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicDecayMode TicBase::getDecayMode()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1138:34: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicInputState TicBase::getInputState()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1154:35: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getInputAfterAveraging()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1164:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getInputAfterHysteresis()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1174:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'int32_t TicBase::getInputAfterScaling()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1190:21: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicMotorDriverError TicBase::getLastMotorDriverError()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1198:41: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicAgcMode TicBase::getAgcMode()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1208:32: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicAgcBottomCurrentLimit TicBase::getAgcBottomCurrentLimit()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1218:46: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicAgcCurrentBoostSteps TicBase::getAgcCurrentBoostSteps()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1228:45: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicAgcFrequencyLimit TicBase::getAgcFrequencyLimit()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1238:42: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint8_t TicBase::getLastHpDriverErrors()':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1249:20: error: 'VarOffset' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::getSetting(uint8_t, uint8_t, uint8_t*)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1268:16: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint8_t TicBase::getVar8(uint8_t)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1330:16: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getVar16(uint8_t)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1337:16: error: 'TicCommand' is not a class or namespace

C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getVar32(uint8_t)':

C:\........\Energia\libraries\tic-arduino-master/Tic.h:1344:16: error: 'TicCommand' is not a class or namespace

Multiple libraries were found for "Tic.h"
 Used: C:\........\Energia\libraries\tic-arduino-master
Multiple libraries were found for "Wire.h"
 Used: C:\.........\Energia15\packages\energia\hardware\msp430\1.0.7\libraries\Wire
exit status 1
Error compiling for board MSP-EXP430F5529LP.

This report would have more information with
"Show verbose output during compilation"
option enabled in File -> Preferences.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~END~~~~~~~~~~~~~~~~~~~~~~~~~~

This is the reply I get from Motor Driver support team Pololu,

"It sounds like the Energia IDE is configured to use a different set of C++ language features than the Arduino IDE. If I enable verbose compilation output in the Arduino IDE 1.8.10, I can see that it passes these arguments to avr-g++ which define what C++ language features are allowed and disable some errors:

-std=gnu++11 -fpermissive --Wno-error=narrowing

If you enable verbose compilation output in the Energia IDE (as mentioned at the bottom of your post) then you should be able to see how it is invoking the compiler, and you should be able to see that those options are either missing or different.

You might be able to look around in the Energia configuration files, find the place where it creates a command for the compiler, and change the options to be like the Arduino IDE. You might find people who faced similar issues on Energia-related forums or by contacting the developers."

I tried to get help from energia forum but couldn't find possible solution to it. 

Can TI help me to sort Library compile errors realted to msp-board and energia?

Energia: 1.8.11E23 (Windows 10), Board: "MSP-EXP430F5529LP" In file included from C:\........\Energia\libraries\tic-arduino-master\examples\I2CMulti\I2CMulti.ino:18:0: C:\........\Energia\libraries\tic-arduino-master/Tic.h:17:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:44:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:65:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:95:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:109:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:120:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:134:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:162:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\libraries\tic-arduino-master/Tic.h:182:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:193:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:209:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:220:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:229:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:241:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:250:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:274:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:286:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:296:1: warning: scoped enums only available with -std=c++0x or -std=gnu++0x [enabled by default] C:\........\Energia\libraries\tic-arduino-master/Tic.h:1281:24: error: ISO C++ forbids initialization of member '_lastError' [-fpermissive] C:\........\Energia\libraries\tic-arduino-master/Tic.h:1281:24: error: making '_lastError' static [-fpermissive] C:\........\Energia\libraries\tic-arduino-master/Tic.h:1281:24: error: ISO C++ forbids in-class initialization of non-const static member '_lastError' C:\........\Energia\libraries\tic-arduino-master/Tic.h:1357:24: error: 'TicProduct' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h:1357:36: error: ISO C++ forbids initialization of member 'product' [-fpermissive] C:\........\Energia\libraries\tic-arduino-master/Tic.h:1357:36: error: making 'product' static [-fpermissive] C:\........\Energia\libraries\tic-arduino-master/Tic.h:1357:36: error: ISO C++ forbids in-class initialization of non-const static member 'product' C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setTargetPosition(int32_t)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:347:16: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setTargetVelocity(int32_t)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:367:16: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::haltAndSetPosition(int32_t)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:388:16: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::haltAndHold()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:409:18: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::goHomeReverse()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:419:15: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::goHomeForward()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:429:15: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::resetCommandTimeout()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:442:18: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::deenergize()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:466:18: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::energize()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:481:18: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::exitSafeStart()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:496:18: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::enterSafeStart()': C:\........\\Energia\libraries\tic-arduino-master/Tic.h:516:18: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::reset()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:530:18: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::clearDriverError()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:548:18: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setMaxSpeed(uint32_t)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:564:16: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setStartingSpeed(uint32_t)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:580:16: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setMaxAccel(uint32_t)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:597:16: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setMaxDecel(uint32_t)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:614:16: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setStepMode(TicStepMode)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:631:15: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setDecayMode(TicDecayMode)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:668:15: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setAgcMode(TicAgcMode)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:678:15: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setAgcBottomCurrentLimit(TicAgcBottomCurrentLimit)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:688:15: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setAgcCurrentBoostSteps(TicAgcCurrentBoostSteps)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:698:15: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::setAgcFrequencyLimit(TicAgcFrequencyLimit)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:708:15: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicOperationState TicBase::getOperationState()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:726:39: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'bool TicBase::getEnergized()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:733:20: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h:734:16: error: 'TicMiscFlags1' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'bool TicBase::getPositionUncertain()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:744:20: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h:745:16: error: 'TicMiscFlags1' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'bool TicBase::getForwardLimitActive()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:751:20: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h:752:16: error: 'TicMiscFlags1' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'bool TicBase::getReverseLimitActive()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:758:20: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h:759:16: error: 'TicMiscFlags1' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'bool TicBase::getHomingActive()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:765:20: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h:766:16: error: 'TicMiscFlags1' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getErrorStatus()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:784:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getErrorsOccurred()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:807:16: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h:808:7: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicPlanningMode TicBase::getPlanningMode()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:827:37: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'int32_t TicBase::getTargetPosition()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:838:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'int32_t TicBase::getTargetVelocity()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:849:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getMaxSpeed()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:860:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getStartingSpeed()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:876:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getMaxAccel()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:892:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getMaxDecel()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:908:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'int32_t TicBase::getCurrentPosition()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:923:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'int32_t TicBase::getCurrentVelocity()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:939:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getActingTargetPosition()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:951:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getTimeSinceLastStep()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:964:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicReset TicBase::getDeviceReset()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:980:30: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getVinVoltage()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:991:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getUpTime()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1005:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'int32_t TicBase::getEncoderPosition()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1016:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getRCPulseWidth()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1034:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getAnalogReading(TicPin)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1054:22: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'bool TicBase::getDigitalReading(TicPin)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1071:32: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicPinState TicBase::getPinState(TicPin)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1090:30: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicStepMode TicBase::getStepMode()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1105:33: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicDecayMode TicBase::getDecayMode()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1138:34: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicInputState TicBase::getInputState()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1154:35: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getInputAfterAveraging()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1164:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getInputAfterHysteresis()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1174:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'int32_t TicBase::getInputAfterScaling()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1190:21: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicMotorDriverError TicBase::getLastMotorDriverError()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1198:41: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicAgcMode TicBase::getAgcMode()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1208:32: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicAgcBottomCurrentLimit TicBase::getAgcBottomCurrentLimit()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1218:46: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicAgcCurrentBoostSteps TicBase::getAgcCurrentBoostSteps()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1228:45: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'TicAgcFrequencyLimit TicBase::getAgcFrequencyLimit()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1238:42: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint8_t TicBase::getLastHpDriverErrors()': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1249:20: error: 'VarOffset' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'void TicBase::getSetting(uint8_t, uint8_t, uint8_t*)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1268:16: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint8_t TicBase::getVar8(uint8_t)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1330:16: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint16_t TicBase::getVar16(uint8_t)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1337:16: error: 'TicCommand' is not a class or namespace C:\........\Energia\libraries\tic-arduino-master/Tic.h: In member function 'uint32_t TicBase::getVar32(uint8_t)': C:\........\Energia\libraries\tic-arduino-master/Tic.h:1344:16: error: 'TicCommand' is not a class or namespace Multiple libraries were found for "Tic.h" Used: C:\........\Energia\libraries\tic-arduino-master Multiple libraries were found for "Wire.h" Used: C:\.........\Energia15\packages\energia\hardware\msp430\1.0.7\libraries\Wire exit status 1 Error compiling for board MSP-EXP430F5529LP. This report would have more information with "Show verbose output during compilation" option enabled in File -> Preferences. ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~END~~~~~~~~~~~~~~~~~~~~~~~~~~

**Attention** This is a public forum