Part Number: MSP430F5437A
Hi,
I am working on MSP430F5437A, and observed that while doing an erase and write to Info D memory, a trail of 0's(24bits) is being written into this memory in between that data. This does not happen always and only happens sometimes and the rest of the data is written properly, except for this trail of 0's in some places. When I extracted the flash memory data, i could see this trail of 0's in several places within the flash(Info D, Flash Bank A etc).
This unexpected trail of 0's in between data is causing unexpected issues. I read that these trail of 0's can occur when there is an overwrite while doing a flash write, but the flash write is being done as mentioned in the flash memory user's guide
Has anyone experienced the same issue?