Part Number: MSP430FR4133
Other Parts Discussed in Thread: MSP-EXP430FR4133, MSP-FET
Hello,
I am using CCS 10.1.0.00010 in Windows with MSP430FR4133 LaunchPad™ Development Kit (MSP-EXP430FR4133)
I am trying to drive the UART from clock derived from XT1.
CS_turnOnXT1(CS_XT1_DRIVE_1);
CS_initClockSignal(
CS_ACLK,
CS_XT1CLK_SELECT,
CS_CLOCK_DIVIDER_1
);
I have XT1 -> ACLK -> TimerA with period of 32767 and duty cycle 16383.
As expected, I see the LED flashing at once per second.
In the same program, the UART works as expected when driven from UCSSEL__SMCLK.
I haven't found a way to drive the UART with ACLK. The choices are:
#define UCSSEL_0 (0x0000) /* USCI 0 Clock Source: 0 */
#define UCSSEL_1 (0x0040) /* USCI 0 Clock Source: 1 */
#define UCSSEL_2 (0x0080) /* USCI 0 Clock Source: 2 */
#define UCSSEL_3 (0x00C0) /* USCI 0 Clock Source: 3 */
#define UCSSEL__UCLK (0x0000) /* USCI 0 Clock Source: UCLK */
#define UCSSEL__MODCLK (0x0040) /* USCI 0 Clock Source: MODCLK */
#define UCSSEL__SMCLK (0x0080) /* USCI 0 Clock Source: SMCLK */
>>>>> How do I drive the UART directly from XT1 -> ACLK?
The underlying problem was the SMCLK/UART data was intermittent when running the code in CCS debug mode.
I was thinking that was really a problem with SMCLK in debug mode and thought XT1 would be a more stable source.
>>>>> Is there another way to fix intermittent SMCLK/UART data in debug mode?
I have an oscilloscope on the bench with board if that is helpful.
Thanks,
Dave