Part Number: MSP430FR2433
Hi E2E,
Good day!
A customer of mine is looking to extend the length of the MSP430 SBW connection. Is there a way to do is? Maybe a buffered SBW, similar to buffered case of 4-wire JTAG?
Best regards,
Franz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR2433
Hi E2E,
Good day!
A customer of mine is looking to extend the length of the MSP430 SBW connection. Is there a way to do is? Maybe a buffered SBW, similar to buffered case of 4-wire JTAG?
Best regards,
Franz
Hi, Franz,
Zrno's idea is correct if you don't request normal speed SWB. It is low cost solution.
It is not good idea to add buffer on SBW signals because the SBW are timing sensitive and the buffer will change the timing for SBW. But if the length for the SBW signals are too long and in case you have to add the buffer, please guarantee the timing specification in section 5.11.10 (debug and emulation) of the MSP430FR2433 datasheet for the 2 pins at package side. Another point need to be taken care is that the RST/SBWTDIO is bi-direction pin for which both input and output timing needs to be checked and the bi-direction buffer also needs to be used.
Thanks,
Lixin
As I said, use the buffer but the delays for the two signals should be similar so as to no violation for the SBW timing specification on the package pins.
Hi All,
My customers cable length would be 3ft. Is slowing the clock sufficient? Also what could be the optimal speed for this?
Thank you for your support.
Best regards,
Franz
Hi Lixin,
Good day!
You may now place this post as resolved.
Thank you for your support.
Best regards,
Franz
**Attention** This is a public forum