This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2155: internal circui of P1.5

Part Number: MSP430FR2155

Hi,

For MPS430FR2155RHA, customer use P1.5 pin as power voltage measurement. below is the circuit:

the problems are :

1, The normal volatge of P1.5 should be 1.14V,  measure the point B, voltage_B is 1.14V, while the voltage_A is 2.4V.

2. if remove the R26, disconnect B and A, measure the point A and B, voltage _B is 1.14V, the voltage_A still 2.4V.

quesiton is what's the internal circuit of P1.5 when it used as analog input? does it be pull up to 2.4V. 

thanks.

**Attention** This is a public forum