Hi Team '432,
I have a customer question..
The Datasheet says “The main memory can be viewed as two independent identical banks of up to 1MB each, allowing simultaneous read or execute from one bank while the other bank is undergoing a program or erase operation.“
In addition, if the Flash erase or program function is located in ROM, then you should be able to erase/program either bank without blocking. However, DriverLib only supports blocking APIs.
What is the preferred method for implementing non-blocking flash erase/program code?
Thanks, Merril