This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5500: Using 2 SPI ports with F5500

Part Number: MSP430F5500


Hello!

I would like to check if what I'm planning is possible.

F5500 has 2 USCI, A1 and B1.

I would lie to use one as slave and one as master, so I will have to remap port 4 because A1CLK is B1STE and B1CLK is A1STE. So I think I will remap either of the STE to P4.7 or P4.7 in order to have independant STE / CLK. Is this possible (i.e. will it work?).

I can't try now, I'm making the PCB, so it would be nice to know it before getting the PCB done.

I'm thinking about this mapping:

P4.0 : A1CLK (no change)

P4.1 : B1MOSI (no change)

P4.2 : B1MISO (no change)

P4.3 : B1CLK (no change)

P4.4 : A1MOSI (no change)

P4.5 : A1MISO (no change)

P4.6 : B1STE

P4.7 : Whatever, possibly PM_NONE.

By the way, PM_NONE allows me to use it a regular GPIO, right?

Thanks,

Pascal

**Attention** This is a public forum