Part Number: EVM430-FR6047
Hello to all,
I have problems to capture the correct paek point from the ADC-captured points to calculate the abs. and delta TOF. The theshold/calculated peak is jumping + or - 1µs (one pulse earlier or later at 1MHz). You can find the parameters and an example of the waveforms below.
Conditions:
Water metering at zero-flow. As you can see the DNS Signal is jumping from 209.6 to 210.6, which is the correct point.
After a while the UPS or DNS Signal jumps again.. Therfore I changed the params "Envelope Crossing Threshold" and "Search Range", but it is all the time the same problem.
Some outliers would be ok, but at the moment its not possible to measure a reliable signal.
What other parameters could I change, in order to improve it?
Thanks for your help.
Regards,
Matthias