Part Number: MSP430FG4619
Tool/software: Code Composer Studio
We are using this very simple SPI code to write to a DAC but the DAC output does not change.
The attached Clock and Data trace show that the clock and data transition are at the exact same instant. No 4ns delay so DAC may be reading garbage. The clock - data lines have a slight delay in all of the spec sheets but not on the trace.
HOW CAN WE DELAY THE CLOCK SO THE DATA CAN SETTLE? Is this the likely problem?
Thanks, Peter
________________________________________________________
#include "main.h"
unsigned int data16,datahi,datalo;
int spi_init (void)
{
P3SEL |= BIT1; // P3.1 UCB0SIMO (Slave in, master out – USCI_B0 SPI mode)
P3SEL |= BIT2; // P3.2 UCB0SOMI (Slave out, master in – USCI_B0 SPI mode)
P3SEL |= BIT3; // P3.3 UCB0CLK (Clock in\out)
IO_OUTPUT(P3,BIT0); //p3.0 CS output
UCB0CTL1 |= UCSWRST; // Put state machine in reset**
UCB0CTL0 |= UCMST+UCSYNC+UCCKPL+UCMSB; // 3-pin, 8-bit SPI master, Clock polarity high, MSB
//UCB0CTL0 |= UCCKPH + UCMSB + UCMST + UCSYNC; // we played with the phase and polarity of clock but not better
UCB0CTL1 |= UCSSEL_2; // SMCLK
//UCB0BR0 = 0x02; // /2 SMCLK=5.2MHZ if div=2 then clock is 2.4Mhz TOO FAST!
UCB0BR0 = 52; // SMCLK=5.2MHZ div=5.2mhz/100,000=52 BR0+BR1x256 so make div=52 for 100K clock
UCB0BR1 = 0;
UCB0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
return 0;
}
/*************************************************************************************/
#define SPI_HDR 0x7000 //0011 bit 16 =0 write bit 15 1=buffered bit 14 GA=1=vref*D/4096 bit 13 SHDC=1
int spi_tx (int spi12bit) { int i;
spi12bit = spi12bit & 0xFFF; //get 12 bits
data16 = SPI_HDR + spi12bit; //MCP4921 header + data
datahi=data16>>8; datalo=data16 & 0xFF;
IO_LOW(P3,BIT0); for(i=0;i<20;i++); //chip select low. wait
UCB0TXBUF = datahi;
while (UCB0STAT & UCBUSY); //wait for finish
UCB0TXBUF = datalo;
while (UCB0STAT & UCBUSY); //wait for finish
for(i=0;i<20;i++); IO_HIGH(P3,BIT0); //chip select high
return 0;
}