This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5342: Sample code to configure a clock generator (SI5341).

Part Number: MSP430F5342


Tool/software: Code Composer Studio

Hi ,

I am new to MSP430 mc .We have a costume zcu111 board of xilinx which have a system controller from TI i,e MSP430F5342 ,a clock generator IC from silicon lab (SI5341) and all of these are interconnected by i2c. This clock generator (SI5341) provides clock to the main CPU (Processing System) and other peripheral like PCIe device .This (SI5341) is a pre configured clock generator ic and the problem we are facing is the main CPU (PS) is not getting clocked  .Our requirement is to programme  the MSP430F5342 system controller via code composer studio which will reconfigure the clock generator ic to our required frequency. Is there any sample code or any support would be helpful .

Thanks in advance

Regards,

Soumya Ranjan

**Attention** This is a public forum